Post Go back to editing

AD9681 ADC Length Matching between the DCO and data lanes - Knobs to tweak

Category: Hardware
Product Number: AD9681

Hi, 

We are designing DAQ board with AD9681 ADC. 

I have one general questions:

1. What should be the length matching requirement between the DCOx clock to Datalanex in the Bank ? 

2. Ideal length matching requirement will be closer to each other. But like to know what difference it will start showing misalignment ? 12.5 mm different is ok or 25 mm ok ? 

Here is the problem in design:

1. Unfortuntely length were focused in our initial board. In bank 2 the length match difference between the data lane and DCO2 become 42 mm. 

2. Question is: Do we have any option in the ADC register it can compensate ?

3. We notice the alignment problem, more frequently. We used FPGA Iserdes IP from xilinx. Is there any expert can help us to tune or set constraints based on the below length matching data points? 

Appericiate immediate help. we like to root cause and find the solution soon to release the product.