Post Go back to editing

ADC Noise floor Understanding

Category: Datasheet/Specs
Product Number: AD9213

Hello,

I have captured ADC Output IQ samples and trying to come up with the noise floor measurement and relating to the noise figure.

I have plotted these IQ data using Visual Analog tool and the plot is below.

I'm not clear how the Average Bin noise is calculated, can you please help me out? If i look at the noise floor, it is about -125dBFS/Hz. However, Average Bin noise is calculated as -133.768dBFS/Hz. How this is derived?

The IQ is captured at 245.76MSPS for 20ms duration.

Parents
  • Hello,

    The equivalent NF of the ADC can be determined as follows:

    1) With a small (or no) signal applied to the ADC such that ADC noise floor is not jitter limited...........,determine the noise floor in dBFS/Hz from the FFT.  In your plot, it is -147.7 dBFS/Hz.  

    2) Calculate what the full-scale input power (i.e. resulting in 0 dBFS reading on FFT) of a sine wave is in dBm while assuming perfect matching).  This is often referred to as PIN_0dBFS. In the case of the AD9213 with a 1.4 Vpp input and 50 ohm RIN, the PIN_0dBFS is  6.9 dBm (i.e. 4.9 mW).

    3) Normalize the ADC noise floor to dBm/Hz (i.e.    = PIN_0dBFS-ADC_Noise_Floor).   The noise floor in dBm/Hz for your plot is -140.8 dBm/Hz ( = 6.9 dBm - 147.7 dBFS/Hz).

    4) The Noise Figure (NF) is the additive noise above thermal noise floor of -174 dBm/Hz at 25 C.  For your plot, the NF = 33.2 dB  (i.e = -140.8 dBm/Hz - (-174 dBm/Hz).

Reply
  • Hello,

    The equivalent NF of the ADC can be determined as follows:

    1) With a small (or no) signal applied to the ADC such that ADC noise floor is not jitter limited...........,determine the noise floor in dBFS/Hz from the FFT.  In your plot, it is -147.7 dBFS/Hz.  

    2) Calculate what the full-scale input power (i.e. resulting in 0 dBFS reading on FFT) of a sine wave is in dBm while assuming perfect matching).  This is often referred to as PIN_0dBFS. In the case of the AD9213 with a 1.4 Vpp input and 50 ohm RIN, the PIN_0dBFS is  6.9 dBm (i.e. 4.9 mW).

    3) Normalize the ADC noise floor to dBm/Hz (i.e.    = PIN_0dBFS-ADC_Noise_Floor).   The noise floor in dBm/Hz for your plot is -140.8 dBm/Hz ( = 6.9 dBm - 147.7 dBFS/Hz).

    4) The Noise Figure (NF) is the additive noise above thermal noise floor of -174 dBm/Hz at 25 C.  For your plot, the NF = 33.2 dB  (i.e = -140.8 dBm/Hz - (-174 dBm/Hz).

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.