AD9213S
Recommended for New Designs
The AD9213S-CSH is a single, 12-bit, 10.25 GSPS, RF analog-to-digital converter (ADC) with a 6.5 GHz input bandwidth. The AD9213S-CSH supports high dynamic...
Datasheet
AD9213S on Analog.com
(1) AD9213's datasheet states that the internal VREF = 0.5V, corresponding to the maximum input voltage Vp-p is 1.4V, it seems that these two values are not related. Theoretically VREF directly determines the ADC input range, and it seems more reasonable to have VREF=0.7V for a differential input range Vp-p of 1.4V, here because of the voltage conversion done?
(2) In addition, the port VREF is connected out on the evaluation board, and we measured the voltage of VREF on the evaluation board drifting between 0.1V~0.25V, is it possible to accurately measure this VREF, or to increase the maximum input voltage range Vp-p by external voltage VREF=0.6V?
Hi Thomas0214
Thanks for your interest in AD9213.
In many ADCs, the reference voltage (VREF) is used to set the full-scale range of the input signal. For the AD9213, I think the internal architecture and gain stages are designed such that a 0.5V VREF results in a 1.4V differential input range. Also, this might be a result of the specific internal scaling and conversion factors used in the ADC design.
Kindly give some time for the product owner () to look into this and provide their response.
Is there a more detailed answer to this question?
Hello,
While scaling factor of 1 or 2x of VREF is often the case.......it need not be that always and can be set by changing gain setting resistors as shown on some other ADC's below. While the AD9213 has a different implementation (i.e. R2/R1 resides is fixed and resides inside the device).............the example below shows that it is possible to have a full-scale input of 1.4 Vpp while having a 0.5 V VREF.
Hello,
While scaling factor of 1 or 2x of VREF is often the case.......it need not be that always and can be set by changing gain setting resistors as shown on some other ADC's below. While the AD9213 has a different implementation (i.e. R2/R1 resides is fixed and resides inside the device).............the example below shows that it is possible to have a full-scale input of 1.4 Vpp while having a 0.5 V VREF.