Hello,
The AD9253 datasheet states the following on page 29:
Data from the output test modes are not necessarily time aligned
from channel to channel. In cases where the output test mode data
is not aligned across all channels, data alignment is restored when
the output test mode bits are disabled and data from the ADC cores
is transmitted in normal functional mode (Register 0x0D = 0x00).
I was planning on using the output test mode to perform word alignment, so I will need at least one channel to have consistent word alignment between the test mode and the ADC core.
Do any of the channels and/or test modes guarantee alignment with the ADC core data?