HI AD Team,
we are using AD9254 with an single-ended input. All in all it's well working, but we had no a couple of ICs, that are showing in our point of view a damage at the input.
After some measurements with full-scale and some overdriven signals, the inputs seems to get damaged.
The Input bias on the VIN+ is than getting lifted. It should stay of course on 0.9V (ideal), but is moving to ~1.2V. This is happening, because the VIN- is delivering a small current, some µA and moving so the bias, to a wrong level.
The ADC is further working, but of course the input signal is offset, due to the unwanted output current from VIN-.
This is the principal input scheme for single ended input.

Absolute Maximum Ratings:
VIN+ to AGND => −0.3 V to AVDD + 0.2 V
Maximum Input is 1V-pp at VIN+ to AGND.
We tried to limit a possible AC-input current at overdrive conditions and changed the input resistor R74 to 1k. However, it's still happening again, that the input is generating another bias.
Also we have seen, that when powering up, there are times, that the input is again ok, but only in the minor case.
We exchanged now around 6 pieces, and experience always the same error after a couple of hours operating (with smaller signals than 1V-pp)!
Any idea, what can cause this?
Please find attached our schematic.


Some other question:
Why is in the datasheet written, that VCM = 0.55 × AVDD, why not 0.5 x AVDD?