KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
HMCAD1520
Production
The HMCAD1520 is a versatile high performance low power analog-to-digital converter (ADC), with interleaving High Speed Modes to increase sampling rate...
Datasheet
HMCAD1520 on Analog.com
Hi,
We have single ended 200 Mhz signal and Nyquist suggests minimum 400MSPS ADC for get 2 Sample. i'd like to get samples more then 2 and i can't upgrade MSPS because of budget. If we use single channel mode , can we clocking in different times to ADC branches to generate multiple samples on one period?
For example,
First branch starts on t time, second is t+1 time third is t+n time(totally 5ns) and finally i'm gonna get to get samples more then 2.
Is it possible for this IC?
I'm begginer to ADC universe so sorry for bad questions.
JEstayo - Moved from Precision ADCs to High-Speed ADCs. Post date updated from Wednesday, October 16, 2024 3:46 PM UTC to Thursday, October 17, 2024 1:22 AM UTC to reflect the move.
Hi,
I have moved this question about hmcad1520 to the High-Speed ADCs forum. Someone here should be able to assist you.
Thanks,
Janine
Hi ZCeyhun
Thanks for using HMCAD1520.
It is capable of running up to 1 GSPS with 8-bit resolution in single channel mode configuration. This done by interleaving the 4 internal ADC to increase the sampling rate. (In Single Channel Mode, one of the four inputs can be selected as valid input to the single ADC channel).

Hi Jalipio,
as far as i understand, If I use single mode 8 bit 1GSPS, IC will work internally 4x250 MSPS and They will be sampling at different times, right? Yes, you are correct.
You may also see Interleaving ADCs: Unraveling the Mysteries | Analog Devices & The ABCs of Interleaved ADCs | Analog Devices for your reference.

Thank you JAlipio.
Best Regards