Post Go back to editing

Same die fabrication process AD9246 and AD9246S?

Category: Hardware
Product Number: AD9246

Is the die fabrication process the same for the regular and aerospace grade version of these parts? 

Thread Notes

Parents Reply
  • Thanks, I was moreso wondering if the die was functionally identical. I have a project that wants to use the AD9246, without concern for total ionizing dose, but there is no radiation test data for that part. If the silicon is identical, then I may be able to approve some allowances based on the single event effect performance oof the AD9246S.

Children
No Data