Post Go back to editing

ADC Selection

Thread Summary

The user is seeking a 2-channel FMC connector-based ADC eval board for ZedBoard with a sample rate >20 MSPS and 12-bit or higher resolution. Analog Devices currently offers reference designs for ZedBoard with the AD9467 (16-bit, 250MSPS), AD9434 (12-bit, 500MSPS), and AD9265 (16-bit, 125MSPS), all of which are single-channel. The EVAL_ADAQ8092 is a 14-bit, 105 MSPS ADC eval board with an FMC connector and available HDL project, but it is a signal chain uModule receiver and not a standard ADC. The user should review the ADAQ8092 datasheet to determine if it meets their application requirements.
AI Generated Content
Category: Hardware
Product Number: ADC

Hi

I am working on an Application that requires ADC. I am looking for a 2 Channel FMC Connector based ADC Eval board for Zedboard.
Sample Rate should be anything more than 20 MSPS.
But I need it with Zedboard and 2 channels are must. Resolution should be 12bit or more. (16bit is very generous)
I am unable to find any such device.


Can anyone share some suggestions

Thanks



Spell
[edited by: imBilal at 10:03 AM (GMT -4) on 1 Oct 2024]

Thread Notes