Post Go back to editing

Why is the AD9642BCPZ-250 not outputting DCO?

Category: Datasheet/Specs
Product Number: AD9642

I am using an LVDS oscillator (DSC1103CL3-250.0000T) as the CLK input for the AD9642. However, the AD9642 is not outputting the DCO signal.

I looked through the register map in the datasheet and couldn’t find any option like “DCO Enable.” Is there any specific reason why the DCO is not working?

Could you help me understand why this might be happening?

  • Hello,

    Please verify the following information:

    1) Ensure AVDD and DRVDD supplies are at 1.8 V at the device pins.

    2) Ensure that the CLK inputs have a DC bias input of 0.9 V  with a differential clock signal exceeding 0.3 Vpp being present.

    3) Ensure that the device is not in a power-down or standby state.

  • 1. As shown in the circuit diagram, AVDD and DVDD are properly inputting 1.8V. I tested register Read and Write via SPI communication.

    2. This is a picture of the input to the CLK pin.

    Diff is 420mVpp, single is 210mVpp. The frequency is input as 250MHz.

    3. The 0x08 register has never been changed from its initial value.
    Should I set it to 0x00 again?

  • Hello,

    You can try resetting via SPI but typically these devices have a Power-on-Reset.  

    Note..........a software reset of all SPI registers to default can be done by setting 0x00 to 0x3C.

    Lastly......other than what I stated above , I am not sure what could be cause unless the voltage levels you show are still insufficient for the CLK receiver input (albeit they look above datasheet spec).  On the last point.....one can try to increase termination resistor to 200 ohms to get an increase in voltage swing from LVDS clock source.

    If this does not work..............someone from ADI factory will need to provide further assistance to you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.