Hello
I have connected AD9083 sysref input to AD9528 out, similar to the evb example PCB (AD9083EBZ).
Now, I found engineer_Note_AD9083 SYSREF interface with LVDS, that suggest different connectivity with level shift circuit.
And the EN also suggest writing to 0xD4C (sysref termination) which is not in the datasheet.
Currently my FPGA recognize the sysref signal but the AD9083 not (reading 0x27E[3:1] return 0).
Is it because of the level shifter? my device reference clock is 200MHz.
Thanks