AD9083
Recommended for New Designs
The AD9083 is a 16-channel, 125 MHz bandwidth, continuous time S-? (CTSD) ADC. The device features an on-chip, programmable, single-pole antialiasing filter...
Datasheet
AD9083 on Analog.com
Thanks for your interest in AD9083.
Your query is acknowledged. Kindly give time for the product owner (jmoreno5) to look into this and provide their response.
Hi taquocviet811 ,
Thank you for reaching out.
May I know your target input bandwidth?
As per datasheet of AD9083, the usable analog input bandwidth is just 125MHz, if your application does not need greater than this then this part is a good choice. AD9083 is a 16 channel ADC, you can utilize all the channel or as you said you only need 8 of it then you can do so.
You can go over with the datasheet of both and feel free to reach out if you need clarification regarding both ADC.
Hi taquocviet811 ,
Here's the answer for your question:
1. Sampling Mode
AD9083 has 16 ADC core. Each ADC has a signal processing tile to filter out of band noise and reduce sampling rate for simultaneous sampling across all channel.
2. Data Rate and JESD Interface
The maximum output data rate is 250MSPS/channel using 8channel. Using below setting:
#Channel =8; L=4; M=8; F=4; S=1; N=16; K=32 with CIC = 8 and J dec = 1
you'll have: (see Table24 of the datasheet)
Fout = 250MHz ; Output Bandwidth = 125MHz
Lane rate = 10Gbps
3. Channel Reduction and Serdes
I think it is feasible. The calculation above shows the lane rate of less than 12.5Gbps. The 16Gbps is the maximum lane rate allowed by the AD9083, Table24 of the datasheet can help you configure your JESD output.