Post Go back to editing

Output Mirror Image from AD9699

Category: Hardware
Product Number: AD9699

Dear Sir,

Our customer is using AD9699 under the following conditions.

  •  Sampling Clock: 2560MHz
  •  NCO Frequency: 640M
  •  DDC: 8
  •  2560M / 8 = 320M sampling
  •  MUX Gain Correction: 6dB
  •  FIR Filter: All path, 6dB Gain Correction
  •  DC Offset Calibration: ON
  •  Input Frequency: 1790MHz

The FFT output is as follows 

  • Signal (-130MHz) -46.7dBm
  • Mirror Image(130MHz) -112.1dBm

Do you have any idea to reduce this Mirror Image? Please advise.

Regards,

Koide

Edit Notes

Corrected typo in the subject, AD969 -> AD9699.
[edited by: masaok at 7:26 AM (GMT -4) on 8 Jul 2024]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.