Post Go back to editing

Common mode voltage for AD9467

Category: Datasheet/Specs
Product Number: AD9467

Is the common mode voltage of AD9467 referred to (VIN+ + VIN- )/2 or the DC bias voltage of VIN+ & VIN-?

If the common mode voltage of AD9467 refers to (VIN+ + VIN- )/2, then I can use different DC bias voltage for VIN+ & VIN-. 

 If the common mode voltage of AD9467 refers to the DC bias voltage, then I need to use the same DC bias voltage for VIN+ & VIN-.

  • Hi JAlipio,

    Therefore, I do not need to worry about the SFDR accordingly.

    BTW, the max. VIN+ & VIN- per my transfer function is 2.7V, exceeding VREF but less than 3.6V. Per AD9467 absolute max. rating, VIN+ & VIN- should be in the range of -0.3V~3.6V.

    Normally, the single end input voltage to the ADC should not exceed VREF such as those sigma delta ADC. But for AD9467, per its max. absolute rating, I think it should be OK. Pls confirm.

    Best regards