Post Go back to editing

Driving multiple AD9236 from an External Voltage Reference

Category: Datasheet/Specs
Product Number: AD9236

I need to drive 6x AD9236. Idea is to reduce system error by using single reference for all of 6 ADC (as recommended in datasheet).
Reference would be buffered with precision OPAMP. Here comes the catch, OPAMPs tend to have stability issues with low Gain (G = 1) and capacitive load.

Datasheet and Evaluation Board Schematics shows 10uF + 100nF capacitors at VREF pin to GND when internal reference is used.
I haven't found an explanation for 10uF cap there. It seems large. Even 100nF is large enough to cause stability issues with OPAMP.
There is no example for external reference.

There would be impulse current it VREF which is not documented. Could you give some explanation what to expect there for current consumption and OPAMP loading?
Could you recommend how to drive AD9236 with external REF buffered, that is with external OPAMP?

Or to keep internal references?

Thanks.