Post Go back to editing

AD6684 what is the configuration for L=1?

Category: Datasheet/Specs
Product Number: AD6684

I7m a DFAE in Japan.

Here is the question from my customer  for AD6684.

Figure 100 in the datasheet shows the example1 setting for "Two ADCs Plus Two DDCs in Each Pair"

The description says "Output serial line rate = 10 Gbps per lane (L = 1) or 5 Gbps per lane (L = 2)"

AD6684 has two ADC pairs(A/B and C/D), each of them has Tx output(physical layer).

what is the configuration in the case of L=1,M=4 ?

Can 4 ADCs connect to one Tx output?