Post Go back to editing

AD9266-80EBZ schematic differences

Category: Datasheet/Specs
Product Number: AD9266

Hello, I recently purchased the evaluation board for the AD9266. It looks like the actual circuit of the optional amplifier input circuitry doesn't match the schematics provided for it, since they are actually based of the AD9649 board. The RLC components don't match what the schematic says at all. Most of the components aren't there, some that shouldn't be (represented as 0Ohm in the schematic) are, although I don't know what their values are... Is the real schematic for the AD9266 available somewhere? I'm specifically referring to this part:

Although I haven't checked if there are more differences. Thanks in advance.

Parents
  • Hello,

    One would need to look at the Bill of Materials (BOM) for the PCB to determine what components are installed and what the values of these components are.  Unfortunately it does not appear that the BOM is provided on the Wiki page link that includes schematics hence someone from the factory would need to provide you with the BOM and also upload to Wiki page.

    Regards

Reply
  • Hello,

    One would need to look at the Bill of Materials (BOM) for the PCB to determine what components are installed and what the values of these components are.  Unfortunately it does not appear that the BOM is provided on the Wiki page link that includes schematics hence someone from the factory would need to provide you with the BOM and also upload to Wiki page.

    Regards

Children