Post Go back to editing

Connecting ADC directly to MCU

Category: Datasheet/Specs
Product Number: AD9649

Hello everyone! I have a task to choose ADC that will have at least 10 MSPS sampling rate and will be able to connect to STM32U575 directly. I very new with this topic, was searching through and found several ones that look like they might work.

Wanted to ask if someone can provide a feedback whether or not following ADC will work in my case, if there is anything else I should consider while using them, etc.

AD9649 Datasheet and Product Info | Analog Devices

Also found these ones, but I do not know if they will work and if yes, whether or not they are better than the first one mentioned above. 

LTC2245 - 14-Bit, 10Msps Low Power 3V ADC (analog.com)

LTC2248/LTC2247/LTC2246 - 14-Bit, 65/40/25Msps Low Power 3V ADCs (analog.com)

If anyone has worked with the better ADC, having similar characteristics, would be great if you could share the information and details!