Post Go back to editing

AD9648 inaccurate reading of register values

Category: Software
Product Number: AD9648
Software Version: spi

读取ad9648的某些寄存器值不准确。请问是我的设置有问题还是IC有问题?我通过SPI写一个寄存器,然后发送0xff、0x01。我写0x03或者0x17写0x81到0x05是正确的,但是很多时候读的时候就不正确  This is me write 0xa5 to 0x17, but read result is 0xb0,,,,,

  这是我写0x81到0x17,读取结果是0x81,正确

 这是我从寄存器0x01读取的内容,其结果应该是0x88。我应该怎么办?

Thread Notes

  • Hi,

    Post translation from Google Translate:

    读取ad9648的某些寄存器值不准确。请问是我的设置有问题还是IC有问题?我通过SPI写一个寄存器,然后发送0xff、0x01。我写0x03或者0x17写0x81到0x05是正确的,但是很多时候读的时候就不正确

    Reading some register values of ad9648 is inaccurate. Is there a problem with my settings or with the IC? I write a register via SPI and send 0xff, 0x01. When I write 0x03 or 0x17, it is correct to write 0x81 to 0x05, but many times it is incorrect when reading.

    这是我写0x81到0x17,读取结果是0x81,正确

    This is when I write 0x81 to 0x17, the read result is 0x81, correct

    这是我从寄存器0x01读取的内容,其结果应该是0x88。我应该怎么办?

    This is what I read from register 0x01, the result should be 0x88. what should I do?

    First of all, could you please write in English, as this community is maintained only in English?

    Second, for support in Chinese, please go to https://ez.analog.com/cn?lang=cn 

    Moved to High-Speed ADCs forum if support in English is good for you.

    Best regards,
    Iulia

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.