Post Go back to editing

latency question

Thread Summary

The user inquired about the meaning of 55 clock cycles in the AD9690 pipeline latency and how to calculate the total latency from analog input to digital output. The final answer clarifies that the 55 clock cycles refer to the ADC pipeline latency, and the datasheet lacks a section to calculate total latency, similar to the AD9208 datasheet. A factory engineer would need to calculate the total latency for the AD9690.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9690

Hi

  1. According to table 4, pipeline latency is 55 clock cycles. Does this clock cycle means the clock which is from CLK+/CLK- pins? Does this pipeline represent the ADC+DSP latency?
  2. How to calculate the consumption time from analog signal inputting AD9690 to digital signal outputting from JESD204B lane?
Parents
  • Hello,

    The specification only refers to the ADC pipeline latency.  The datasheet is lacking a section similar to what is shown in the AD9208 datasheet as shown below which would allow one to calculate total latency.  Someone from factory would need to calculate latency for AD9690 since this section does not exist on the AD9690 datasheet.

Reply
  • Hello,

    The specification only refers to the ADC pipeline latency.  The datasheet is lacking a section similar to what is shown in the AD9208 datasheet as shown below which would allow one to calculate total latency.  Someone from factory would need to calculate latency for AD9690 since this section does not exist on the AD9690 datasheet.

Children
No Data