Post Go back to editing

AD9629 noise and sample code

Category: Software
Product Number: AD9629
Software Version: code

HI 

  I have encountered some problems with the ADC, the input sine wave, the acquired digital signal is divided into two parts, and the noise is obviously, what is the problem, can you provide an example code?THX SO MUCH!

#include "ad9629.h"
#include "assert_profile.h"
#include <stddef.h>

uint8_t read_data = 0;
void ad9629_adapter_init(AD9629_ADAPTER_STR * p_adapter)
{
    ASSERT_ERROR(p_adapter != NULL);
    ASSERT_ERROR(p_adapter->p_read_reg != NULL);
    ASSERT_ERROR(p_adapter->p_write_reg != NULL);
    ASSERT_ERROR(p_adapter->p_start_sample != NULL);
    ASSERT_ERROR(p_adapter->p_stop_sample != NULL);
    
    p_adapter->p_write_reg(0x00, 0x3C);//soft reset
    
    read_data = p_adapter->p_read_reg(0x01);//read id
//    ASSERT_ERROR(read_data == 0x70);
    
    read_data = p_adapter->p_read_reg(0x02);//read unique speed
    
    p_adapter->p_write_reg(0x0B, 0x01);//divide by 2
    
//    p_adapter->p_write_reg(0x0D, 0x48);//test mode
//    p_adapter->p_write_reg(0x19, 0xAA);
//    p_adapter->p_write_reg(0x1A, 0x0A);
//    p_adapter->p_write_reg(0x1B, 0x55);
//    p_adapter->p_write_reg(0x1C, 0x05);
    
    p_adapter->p_write_reg(0x14, 0x01);//output format: twos complement
//    p_adapter->p_write_reg(0x08, 0x60);//normal mode:output enable
    
    p_adapter->p_write_reg(0xFF, 0x01);
//    read_data = p_adapter->p_read_reg(0x0B);
//    read_data = p_adapter->p_read_reg(0x08);

//    read_data = p_adapter->p_read_reg(0x19);
//    read_data = p_adapter->p_read_reg(0x1A);
//    read_data = p_adapter->p_read_reg(0x1B);
//    read_data = p_adapter->p_read_reg(0x1C);

//     p_adapter->p_write_reg(0x08, 0x60);    //enable pin23 output mode
}

void ad9629_start_sample(AD9629_ADAPTER_STR * p_adapter)
{
    ASSERT_ERROR(p_adapter->p_start_sample != NULL);
    
    p_adapter->p_start_sample();
}

void ad9629_stop_sample(AD9629_ADAPTER_STR * p_adapter)
{
    ASSERT_ERROR(p_adapter->p_stop_sample != NULL);
    
    p_adapter->p_stop_sample();
}