Hi,
I am trying to design a baseband network operating at 10MHz. My system is using the AD8376 differential VGA to drive a AD9259 ADC.
I am trying to design the output network for the AD8376 (selecting the correct bias resistors) but I can't seem to find the differential input load of the AD9259 on the datasheet. I can see that the input capacitance of the inputs is 7pf (screenshot attached), but there is no mention of the input impedance. Do I assume it is high impedance? Or if I'm driving 100Ohm differential lines, will RL = 100?
![]()
For reference I am looking at the AD8376 datasheet and trying to perform the following:

Thanks,
Louis