Hello
I am building a board with 3 AD9697 connected to a Kintex Ultrascale. The R/O is working well.
The ADC inputs are DC coupled and I use the Vref pin to get the VCM from the ADC to feed to ADA4927 single-to-diff amplifier.
When measuring the Vcm from different ADC, one is giving 1.41V as expected but the second is giving 1.77V and the third one 1.57V.
I am wondering if such a spread is expected with the chosen ADC or if I have to investigate for broken things on my board.
Thank you in advance for your help.
Best regards,
Marc