Post Go back to editing

vcm spread with AD9697

Thread Summary

The user encountered inconsistent common mode voltages (Vcm) across three AD9697 ADCs when using DC coupling. The solution involved adjusting the buffer current settings by writing specific values to registers 0x18e0, 0x18e1, and 0x18e2, which improved Vcm consistency and signal baseline stability. The final configuration for 0x18e3 was 0x4f, not 0x40, to avoid a Vcm of 0.8V. The user also noted that the AD9697 datasheet is outdated and referred to the AD9695 datasheet for register descriptions.
AI Generated Content
Category: Hardware
Product Number: AD9697
Software Version: N/A

Hello

I am building a board with 3 AD9697 connected to a Kintex Ultrascale. The R/O is working well.

The ADC inputs are DC coupled and I use the Vref pin to get the VCM from the ADC to feed to ADA4927 single-to-diff amplifier.

When measuring the Vcm from different ADC, one is giving 1.41V as expected but the second is giving 1.77V and the third one 1.57V.

I am wondering if such a spread is expected with the chosen ADC or if I have to investigate for broken things on my board.

Thank you in advance for your help.

Best regards,

Marc

  • Hi Marc,

    Thanks for your interest in AD9697. 1.4V is the correct common mode voltage. Could you provide your SPI writes for the DC coupling configuration?

    To export the common-mode voltage to the VREF pin need write some additional registers through SPI.

    Regards,

    Alvin

  • Thank you for your response.

    What I write so for is :

    Reg 0x1908 -> 0x04 : analog input optimized for DC coupling
    Reg 0x18a6 -> 0x00 : Vref internal
    Reg 0x18e6 -> 0x00 : Temp diode High Z
    Reg 0x1910 -> 0x0d : 1.7V pp input
    Reg 0x18e3 -> 0x4f : external Vcm buffer + some unknown parameter
    Reg 0x1a4c -> 0x0f : Buffer current P : 300 uA (don't know what it means)
    Reg 0x1a4d -> 0x0f : Buffer current N : 300 uA (don't know what it means)
    Reg 0x1b03 -> 0x02 : Buffer control 3 (as in the datasheet)
    Reg 0x1b08 -> 0xc1 : Buffer control 4 (as in the datasheet)
    Reg 0x1b10 -> 0x00 : Buffer control 5 (as in the datasheet)
    Reg 0x0561 -> 0x00 : offset binary, not inverted

    Some parameters are taken from the datasheet, even if I don't understand in details what they really means as "buffer control".

    Best regards

    Marc

  • Hi Marc,

    Thanks for the update.

    Could you try below writes:

    Reg 0x1908 -> 0x04 : analog input optimized for DC coupling
    Reg 0x18a6 -> 0x00 : Vref internal
    Reg 0x18e6 -> 0x00 : Temp diode High Z
    Reg 0x1910 -> 0x0d : 1.7V pp input

    Reg 0x18e0 -> 0x02 : 
    Reg 0x18e1 -> 0x14 : 
    Reg 0x18e2 -> 0x14 :
    Reg 0x18e3 -> 0x40 :

    Reg 0x18e3 -> 0x4f : external Vcm buffer + some unknown parameter
    Reg 0x1a4c -> 0x0f : Buffer current P : 300 uA (don't know what it means)
    Reg 0x1a4d -> 0x0f : Buffer current N : 300 uA (don't know what it means)
    Reg 0x1b03 -> 0x02 : Buffer control 3 (as in the datasheet)
    Reg 0x1b08 -> 0xc1 : Buffer control 4 (as in the datasheet)
    Reg 0x1b10 -> 0x00 : Buffer control 5 (as in the datasheet)
    Reg 0x0561 -> 0x00 : offset binary, not inverted

    Please let me know if it works on your board.

    Regards,
    Alvin

  • Great !

    I have added the setting of registers 0x18e0, 0x18e1 and 0x18e2 but kept the content of 0x18e3 to 0x4f and not 0x40 and it works much better.

    Now I have 1.40V, 1.41V and 1.38V for Vcm of the 3 ADCs.
    With 0x18e3 set at 0x40, I got 0.8V for Vcm which is not the expected value. I have understood that the 6 lsb of this register are setting a current in a buffer. I guess that this current should not be 0.

    By the way I have not seen the description of registers 0x18e0, 0x18e1 and 0x18e2 in the datasheet. My version is Rev.0. I have not found newer versions.

    The by-product of the new setting is also curing a problem I was fighting for a while : very low frequency instability of the baseline of the signal. Now, it is much more stable. I am looking for unipolar pulses, so the base line has to be set near the lower or upper rail of the ADC depending of the pulse sign.

    Thank you very much for your very valuable help which make me a (big) step closer to a working board.

    Best regards,

    Marc

  • OK, the registers are described in the datasheet of AD9695. A new Rev of AD9697 datasheet could be useful. If I remember well, I have found some small typo in the Rev0 which should be corrected.

    Marc

  • Hi Marc,

    Good to know it works. Thanks for the updating.

    Thanks for the update. Please refer to ad9695 datasheet for now, the datasheet of ad9697 is in the queue waiting to be edited. It's recommended to write 0x18e3[6] first, then write 0x18e3[5:0] as I attached earlier, the input common mode voltage will slightly change based on the buffer current settings.

    Reg 0x18e3 -> 0x40 :

    Reg 0x18e3 -> 0x4f : external Vcm buffer + some unknown parameter

    Regards,

    Alvin

  • Sorry, I have been off for few days.
    I would like to thank you very much for your help again !

    best regards

    Marc

  • Just a gentle reminder that promises to update the AD9697 data sheet, which is still at Rev 0 on a part from 2018, have been made regularly for about 6 years now...

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.