AD9208 has a small signal at FS/4 and the small signal amplitude will change when resetting the JESD bus. ADC cannot be powered off. The ADC configuration is dual -channel DDC mode, L = 8, F = 1, M = 2. ADC sampling rate 3Gbps, FFT points 1047586, DDC is FS/4Hz IF mode. Sometimes the amplitude is large, exceeding 20dB of noise and sometimes the amplitude is small, only exceeding the noise 5 ~ 10dB. If the JESD bus of the ADC is not reset, the small signal amplitude will not change. The specific configuration of the ADC is:
0x0000 0x81
0x0000 0x00
0x0002 0x00
0x0008 0x03
0x0200 0x02
0x0201 0x01
0x0550 0x00
0x0327 0x05
0x0701 0x86
0x0347 0x05
0x0040 0x00
0x0245 0x01
0x0247 0xFF
0x0248 0x1F
0x0249 0x00
0x024A 0x10
0x024B 0xFF
0x024C 0x00
0x0310 0x63
0x0311 0x05
0x0330 0x63
0x0331 0x05
0x1910 0x0E
0x1A4C 0x19
0x1A4D 0x19
0x0571 0x15
0x058E 0x03
0x058F 0x8F
0x058B 0x07
0x058C 0x01
0x1228 0x4F
0x1228 0x0F
0x1222 0x00
0x1222 0x04
0x1222 0x00
0x1262 0x08
0x1262 0x00
0x0571 0x14
After the ADC is powered on, all the content is configured for the first time. The second configuration only configures 0x0571 to write 0x15, 0x0571 to write 0x14. A small signal amplitude will change a lot. If Jesd is not reset, the small signal does not change. Help analyze what the reason is, thank you.