Post Go back to editing

FPGA source code AD9681 + HSC - ADC - EVALEZ

Thread Summary

The user requested FPGA source code for the HSC-ADC-EVALEZ (Virtex 6) board with AD9681, including examples for USB-PC communication. The support engineer provided the code after verifying the user's email address. The user now seeks examples or APIs for real-time data processing and host computer receiving code, and has successfully collected data using MATLAB but lacks the ADSP-BF527KBCZ source code.
AI Generated Content
Product Number: AD9681 capture board HSC - ADC - EVALEZ

Hello,

           I am working with  HSC-ADC-EVALEZ +AD9681. Now my work is to program the FPGA on HSC-ADC-EVALEZ (Virtex 6). Whether is there any source code for this board? both VHDL and verilog is better.

           Thank you so much!

Parents Reply
  • Hi Jxav,

    I'm sorry I missed your message earlier.

    I need FPGA source code about AD9681 and HSC - ADC - EVALEZ (Virtex 6). It is even better if the code source is on the vivado

    platform.

    In addition, I am really concerned about the part about the communication between USB and PC, and I would be grateful if

    you could provide relevant information.

    Thank you.

    JSA

Children
No Data