How to trigger AD9249 sampling (Control start?
moved and updated form
[edited by: GenevaCooper at 1:09 PM (GMT -4) on 11 Aug 2023]
AD9249
Recommended for New Designs
The AD9249 is a 16-channel, 14-bit, 65 MSPS analog-to-digital converter (ADC) with an on-chip sample-and-hold circuit that is designed for low cost, low...
Datasheet
AD9249 on Analog.com
How to trigger AD9249 sampling (Control start?
Hi China542,
Thanks for your interest in AD9249.
Can you provide additional details? Do you mean external triggering of AD9249? Do you use an evaluation board?
Regards,
Xavier
Thank you very much for your answer. Specifically, I want to use the AD9249 to sample the signal collected by the front end, and I need to determine at what time the signal is being collected, in other words, I want to be able to control the moment at which it is sampling. I checked the manual for the AD9249 and could not find an interface to connect to external triggers. In addition, we need to use an evaluation board. Looking forward to your reply again.
Thank you very much for your answer. Specifically, I want to use the AD9249 to sample the signal collected by the front end, and I need to determine at what time the signal is being collected, in other words, I want to be able to control the moment at which it is sampling. I checked the manual for the AD9249 and could not find an interface to connect to external triggers. In addition, we need to use an evaluation board. Looking forward to your reply again.