Is it possible to Interface AD9680 with Digilent Genesys 2 Kintex®-7 FPGA Development Board ? Thanks.
AD9680
Recommended for New Designs
The AD9680 is a dual, 14-bit, 1.25 GSPS/1 GSPS/820 MSPS/500 MSPS analog-to-digital converter (ADC). The device has an on-chip buffer and sample-and-hold...
Datasheet
AD9680 on Analog.com
Is it possible to Interface AD9680 with Digilent Genesys 2 Kintex®-7 FPGA Development Board ? Thanks.
Sorry, There is a typo. Please read it as "Is it possible to Interface AD9680-LF1000EBZ Evaluation board with Digilent Genesys-2 Kintex®-7 FPGA Development Board ?"
Hi PRA360,
Thank you for your interest in AD9680.
You may refer to this wiki guide for the evaluation of AD9680 using ADS7-V2.
EVALUATING THE AD9680/AD9690/AD9234 ANALOG-TO-DIGITAL CONVERTER [Analog Devices Wiki]
The reference hardware design files are available here for your reference.
We can provide the reference FPGA source code. Let us know if you want to get a copy, just make sure to provide a correct information on your profile.
Best regards,
Peevee
Hi Peevee,
Thanks for the reply. I had gone through the suggested guide where the details of evaluation of AD9680 using ADS7-V2 are mentioned. However, for interfacing several other peripherals along with AD9680, we have to use Digilent's Genesys 2 Kintex®-7 FPGA Development Board for the desired DSP. In this context, wanted to make sure whether the above interfacing is okay or not. I mean, would there be any hardware or software/firmware compatibility issue ? I would be grateful to you if you share some information on it.
Hi Peevee,
Thanks for the reply. I had gone through the suggested guide where the details of evaluation of AD9680 using ADS7-V2 are mentioned. However, for interfacing several other peripherals along with AD9680, we have to use Digilent's Genesys 2 Kintex®-7 FPGA Development Board for the desired DSP. In this context, wanted to make sure whether the above interfacing is okay or not. I mean, would there be any hardware or software/firmware compatibility issue ? I would be grateful to you if you share some information on it.