Post Go back to editing

LTC2249 Input range

Thread Summary

The user asked if the LTC2249 ADC's full scale range is 7dBm for ±1V mode with 100-ohm input impedance, and if the minimum input power level is -66dBm due to a 73dB SNR. The support engineer confirmed the full scale range is 6.99dBm but clarified that the SNR is in dBFS, not dBm, and the analog signal is -1dBFS as per test conditions.
AI Generated Content
Product Number: LTC2249

Hi

According to LTC2249 datasheet for the ±1v mode (V sense connect to Vdd), is the ADC's full scale range 7dBm for a 100-ohm input impedance ?

Due to a 73dB SNR is the minimum input power level of ADC -66dBm?

Best regard

Parents
  • Hi jessi,

    Thanks for your interest in LTC2249.

    According to LTC2249 datasheet for the ±1v mode (V sense connect to Vdd), is the ADC's full scale range 7dBm for a 100-ohm input impedance ?

    Yes, this is correct. The ADC full-scale swing is 2Vpp and is equivalent to 6.9897dBm for 100-ohm input impedance.

    Due to a 73dB SNR is the minimum input power level of ADC -66dBm?

    No. The SNR parameter is in dBFS scale, and not should be interpreted in dBm. SNR (dBFS) = Signal (dBFS) - Noise (dBFS)

    As for the 73dBFS SNR, the analog signal is -1dBFS as per test conditions.

    Regards,

    Xavier

Reply
  • Hi jessi,

    Thanks for your interest in LTC2249.

    According to LTC2249 datasheet for the ±1v mode (V sense connect to Vdd), is the ADC's full scale range 7dBm for a 100-ohm input impedance ?

    Yes, this is correct. The ADC full-scale swing is 2Vpp and is equivalent to 6.9897dBm for 100-ohm input impedance.

    Due to a 73dB SNR is the minimum input power level of ADC -66dBm?

    No. The SNR parameter is in dBFS scale, and not should be interpreted in dBm. SNR (dBFS) = Signal (dBFS) - Noise (dBFS)

    As for the 73dBFS SNR, the analog signal is -1dBFS as per test conditions.

    Regards,

    Xavier

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.