Post Go back to editing

AD9680 IBIS AMI

Category: Software
Software Version: ADS 2022

AD9680 AMI MODEL on-die s-parameter ss/ff/tt in the SNP file is representing the slow/fast/typical? The SNP file port 1 2 3 4,which 2 ports are the differential input,which 2 ports are the differential output,corresponding to n and p .

There are 15 ports in the packaged snp file, the port 1/2/3 is connected to the gnd net. Which net name in package pin map corresponds to port 4 through 9 and port 10 through 15?