Post Go back to editing

AD9680 IBIS AMI

Category: Software
Software Version: ADS 2022

AD9680 AMI MODEL on-die s-parameter ss/ff/tt in the SNP file is representing the slow/fast/typical? The SNP file port 1 2 3 4,which 2 ports are the differential input,which 2 ports are the differential output,corresponding to n and p .

There are 15 ports in the packaged snp file, the port 1/2/3 is connected to the gnd net. Which net name in package pin map corresponds to port 4 through 9 and port 10 through 15?

Parents Reply Children on Jun 5, 2023 2:49 AM in reply to mark8

Hi,

You may refer to the AD9680 product page AD9680 Datasheet and Product Info | Analog Devices under Tools & Simulations to download the IBIS-AMI model of AD9680.

Regards,

Meriam