Hi,
I want to send serialized data from AD9250 output through optical fiber, which uses JESD204B protocol. I have 2 serial lanes of 5 Gbps each , 1 sampling clock of 250 MHz, and one SYNC signal which is basically a reset signal.
I want to send all of these 4 signals through optical fiber to an FPGA development board (Terasic HAN pilot) but as you can see they have pretty much different bandwidth, from 5Gbps CML driver, to SYNC signal which is a DC "ON" or "OFF" signal.
The HAN Pilot board provides 4 SFP+ transceiver 10 GBe connectors. So my question is, can I use the SFP+ 10 Gbe to send the 5 Gbps signals, the 250 MHz one, and the DC one ? Is the 10 Gbps fixed by SFP+ module, or is there a low frequency / low data rate limit ? I speak for SFP+ optical fiber module, and not copper câble modules, because I know some optical fiber transmitters are AC coupled pretty high in frequency, and they cannot send lower frequency data. But for SFP+ standard I couldn't find any documentation mentioning this ?
Thanks,
Rleduc
Missing word
[edited by: Rleduc at 2:42 PM (GMT -4) on 3 May 2023]