Hello support team,
I have gone through the reference schematic of the AD9653 evaluation board. In that, I have an query related to AD9653 front end circuit.
As per ETC1-1-13 datasheet, pin 5 is the secondary dot port and pin 1 is primary dot port. but in schematic, pin 5 is mentioned as primary port and pin 1 as secondary port. Also, input_A+ connection is interfaced with only ADT1-1WT+ but it is mentioned as DNI. request you to please provide guidance on front end circuit which will be there in the evaluation board?