Post Go back to editing

Bandwdith of AD6684

Category: Datasheet/Specs
Product Number: AD6684

Hi,

I have a very basic question regarding bandwidth of AD6684 IF Receiver. The specifications document says it's a 135MHz Quad IF receiver. The block diagram of the receiver shows, 4 paths each consisting of a 500MS/s ADC, and DDC with NSR and VDR options available. Each DDC has 4 half band filters so with one half band filter enabled, output IQ rate would be 250MS/s and the alias rejected band is of 200MHz. What does 135MHz bandwidth represent then ? I see no filter even before ADC in the block diagram. What is the significance of this 135MHz Bandwidth ?

Thanks 

Parents Reply Children
No Data