Post Go back to editing

AD9254 SPI port

Product Number: AD9254

The manual of AD9254 states that the voltage range of SCLK pin or CSB pin is less than 3.6V, but there is a pull-up resistance in the CSB pin to AVDD, and the voltage of AVDD is 1.8V. In this way, when we use 3.3V SPI interface, if DVDD uses 2.5V and AVDD uses 1.8V, can CSB and SCLK pin directly use 3.3V logic level to access the chip without level conversion? If used directly, 3.3V power will leak to AVDD through pull-up resistance. Does it affect chip performance? . And it says in the manual that if SPI is not used, the CSB pin should be pulled up to AVDD.



regards
[edited by: joshxu at 7:48 AM (GMT -5) on 23 Feb 2023]