Hello,
I have a question from our customer about the function of GPIO_x1 of AD9689.
He is going to assign MNTO output to GPIO_A1 pin but can not get MNTO signal.
I found the same question on ez.analog.com/.../414904 but this thread was not answered.
I am paying attention table-3 and table-8, figure-77
1. In table-3, GPIO_A1 and GPIO_B1 have LOGIC INPUTS specifications but do not have specifications of LOGIC OUTPUTS.
2. In table-8, GPIO_A1 and GPIO_B1 are described as input/output functions.
3. In figure-77, GOIP_A1 and GPIO_B1 are drawn as input function.
I think table-3 and figure-77 are indicated GPIO_A1 and GPIO_B1 have only input functions.
Do GPIO_A1 and GPIO_B1 have output functions?
Best regards,
y_suzuki
corrected the writing error.
[edited by: y_suzuki at 2:50 AM (GMT -5) on 10 Feb 2023]