Post Go back to editing

Question bout AD9226 Output Enable

Category: Datasheet/Specs
Product Number: AD9226

Hi,

I have a question about the OUTPUT ENABLE specification listed in the AD9226 data sheet.

I assume that the "Low" threshold of OUTPUT ENABLE is (DRVDD/2)-0.5 (V), is this correct?

What is the specification for the max value: (DRVDD/2)+0.5 (V)?

Kazu

Parents Reply
  • Hi Xavier,

    I have an additional question on AD9226. In the datasheet 48-PIN FUNCTION DESCRIPTIONS, pins 5, 6, 8, 10, 11, and 44 are NC.

    On the other hand, in the schematic in Figure 21, pin 5 is connected to GND, and pins 10 and 11 are connected to U7 (74VHC541)

    in Figure 22.

    Are pins 5, 10, and 11 NC? Or should I follow the schematic?

    Regards,

    Kazu

Children