Post Go back to editing

AD9226 Input Span

Category: Datasheet/Specs
Product Number: AD9226

Hi

I am DFAE in Japan.

Input Span is 2Vp-p at VREF=2V according to AD9226 Datasheet.

Is it OK for VINA to amplitude from 2V to 4V and VINB to amplitude from 4V to 2V?

Then “VINA-VINB” amplitude from -2V to +2V.

Best regards

N.Kokubo

Top Replies

Parents
  • Hi Kokubo-san,

    Input span is 2Vp-p at VREF=2V.

    At common-mode voltage = 3V, VINA should swing from 2.5V to 3.5V & VINB should swing from 3.5V to 2.5V.

    VINA-VINB should be from -1V to +1V.

    See sample image below for your condition based on Figure 7 from the datasheet.



    Best regards,
    Peevee

  • Hi Peevee -san,

    Thank you for prompt reply.

    Input span is 2Vp-p at VREF=2V and VINA swings from 2.5V to 3.5V & VINB swings from 3.5V to 2.5V.

    VINA-VINB swings from -1V to +1V.

    Then Binary Code does not swing from 0000 0000 0000 to 1111 1111 1111 1111.

    Binary Code swing only from 0100 0000 0000 to 1011 1111 1111 according to Table IV in AD9226 Datasheet.

    Is my understanding correct?

    Best regards,
    N.Kokubo

Reply
  • Hi Peevee -san,

    Thank you for prompt reply.

    Input span is 2Vp-p at VREF=2V and VINA swings from 2.5V to 3.5V & VINB swings from 3.5V to 2.5V.

    VINA-VINB swings from -1V to +1V.

    Then Binary Code does not swing from 0000 0000 0000 to 1111 1111 1111 1111.

    Binary Code swing only from 0100 0000 0000 to 1011 1111 1111 according to Table IV in AD9226 Datasheet.

    Is my understanding correct?

    Best regards,
    N.Kokubo

Children