Post Go back to editing

About the /OE terminal function and timing diagram of LTC2202/LTC2203

Category: Datasheet/Specs
Product Number: LTC2203

Hello everyone

I am planning to use LTC2202/LTC2203 to get a fixed number of samples periodically.

Since there is an output enable pin /OE, and the datasheet states that /OE high level puts "digital outputs" in Hi-Z state, I think maybe I can pull up its level after counting a certain number of CLKOUT+ rising edges.

I'm not sure if the /OE high level disables both CLKOUT+ and D0~D15(sample output terminals)   or only the D0~D15?

And the datasheet has no timing diagram about /OE terminal, but I think there may be an output delay(or set up time) for sample output terminals to be valid after the /OE falling edge.

Is there any other user guide or design reference in which I can find the output delay time ?

I would appreciate it if you could reply.

Best regards,

Alaudi

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.