Hi!
We are Planning to use Multiple AD9253-105 (across Boards) with Length matched Sampling clock to achieve Phase Matching.
Our Requirement are as follows,
Output Freq: 75MHz
Sampling Freq: 100MHz(no divider is utilized in ADC)
Phase matching: <30ps
Query:
1)Is it possible to achieve our Phase matching Requirement with the selected part AD9253-105?
2) What would be Part to part Latency variation? will this latency be deterministic or will it vary from Power on to Power ON based on Temperature and Voltages?
3)Please share the Test Results demonstrating Phase matching Accuracy using AD9253-105.
Thanks in-advance,
Deva