AD9213's SYNCINB_x signal must be DC-coupled?
AD9213
Recommended for New Designs
The AD9213 is a single, 12-bit, 6 GSPS/10.25 GSPS, radio frequency (RF) analog-to-digital converter (ADC) with a 6.5 GHz input bandwidth. The AD9213 supports...
Datasheet
AD9213 on Analog.com
AD9213's SYNCINB_x signal must be DC-coupled?
Hi daidaishannon,
Yes, AD9213's SYNCINB signal, and JESD204B SYNC signals in general, should be DC-coupled. This is not so much a device requirement but rather it is a system requirement. The JESD204B SYNC signals are asserted when needed and otherwise will be idle. Long idle periods can be an issue when AC coupled.
Thank you.
Doug
Hi daidaishannon,
Yes, AD9213's SYNCINB signal, and JESD204B SYNC signals in general, should be DC-coupled. This is not so much a device requirement but rather it is a system requirement. The JESD204B SYNC signals are asserted when needed and otherwise will be idle. Long idle periods can be an issue when AC coupled.
Thank you.
Doug