AD9213's SYNCINB_x signal must be DC-coupled?
AD9213
Recommended for New Designs
The AD9213 is a single, 12-bit, 6 GSPS/10.25 GSPS, radio frequency (RF) analog-to-digital converter (ADC) with a 6.5 GHz input bandwidth. The AD9213 supports...
Datasheet
AD9213 on Analog.com

AD9213's SYNCINB_x signal must be DC-coupled?
Hi daidaishannon,
Yes, AD9213's SYNCINB signal, and JESD204B SYNC signals in general, should be DC-coupled. This is not so much a device requirement but rather it is a system requirement. The JESD204B SYNC signals are asserted when needed and otherwise will be idle. Long idle periods can be an issue when AC coupled.
Thank you.
Doug