KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
AD8138
Production
The AD8138 is a major advancement over op amps for
differential signal processing. The AD8138 can be used as a
single-ended-to-differential amplifier or...
Datasheet
AD8138 on Analog.com
AD9283
Production
The AD9283 is an 8-bit monolithic sampling analog-to-digital converter with an on-chip track-and-hold circuit and is optimized for low cost, low power...
Datasheet
AD9283 on Analog.com
Newbie designer here. I'm trying to design a circuit to interface a 1 Vpp (into 75 ohm) video signal DC-coupled via a AD8138 to a AD9283. I used DiffAmpCalc to design an input stage around the AD8138 (see screenshot). The AD8138 is powered by a +3.3V and a -3.3V LDO regulator; the +3.3V regulator also powers the analog side of the AD9283 (Vd).
At the output of the AD8138, DiffAmpCalc shows a 0.490 Vpp signal centered around Vocm on both the positive and the negative output. The differential voltage between the outputs, ie. VoutP - VoutN, would then be 1 Vpp centered around Vocm.
Now, the AD9283 datasheet mentions in the specifications:
I don't understand the input voltage range specification. I think it agrees with the output voltages of the AD8138 described above. Is that correct? Why does it say +/- 512 mV peak-to-peak (or p-p)?
Regarding the common mode voltage (Vocm), I've set it to 0.99 V in DiffAmpCalc, i.e. 0.3 * Vd, as mentioned here Common-mode voltage AD9283-100. However, I'm not enitrely sure how this relates to the +/- 200 mV specification for the common mode voltage. Also, what is better, 0.9V or 0.99 V, or can I simply use 1V? I guess that in practice it may be difficult to supply exactly 0.99V?

Hi 0xa000,
Thanks for your interest in AD9283.
Now, the AD9283 datasheet mentions in the specifications:
- Input voltage range (with respect to Ain) of +/- 512 mV p-p
- Common-mode voltage +/- 200 mV
Input voltage range (with respect to Ain) relates to the differential AC signal with typical value of +/-512mVpp or 1.024Vpp for AD9283. If you relate that one to the Diff-Amp, it means Vspp given that the Vsdc = 0V.
Why does it say +/- 512 mV peak-to-peak (or p-p)?
The +/-512mVpp is the optimized full-scale input range. This value also the basis for the dynamic performance measurements according to footnote 5 in the datasheet.

Common-Mode Voltage means the DC voltage required by AIN pin. With reference to 0.3*Vd or 0.3*3.0V equal to 900mV which is the typical Vcm, the +/- 200mV values will give the allowable range as stated below:
However, I'm not enitrely sure how this relates to the +/- 200 mV specification for the common mode voltage. Also, what is better, 0.9V or 0.99 V, or can I simply use 1V? I guess that in practice it may be difficult to supply exactly 0.99V?
Either 0.9V or 1V is allowed since it falls under 0.7V or 1.1V. You can refer to the figure below or these links below:
MT-075: Differential Drivers for High Speed ADCs Overview (analog.com)

Regards,
Xavier
Hi Xavier,
Thanks for your reply! I'll have a look at the links you mentioned.
Your DiffAmpCalc screenshot looks at bit different from mine. In my case, the input signal is always above ground. When I measure the source signal terminated into a 75 ohm resistor to ground, what I get is 1 Vpp + 0.5 Vdc. So, I used a Vspp of 2V, Vsdc of 1 V, 75 ohm source resistance, and 75 ohm termination in DiffAmpCalc to match these measurements.
Then I try to subtract the 0.5 Vdc via the inverting input, and use a gain of 0.5x and a Vocm of 1V to (I hope) match the output voltages to the range that the AD9283 expects.
But I'm not really sure what I'm doing... :-)
The voltages on the output (VoutN, VoutP) we get are the same, though. And these are in line with the AD9283 specs right?
Regards,
Joris
Hi Joris,
Sorry for the late reply.
Here are my points from ADC's point of view (not really a DiffAmp expert :))
Thank you and regards,
Xavier
Hi Xavier,
Thanks! It's not uncommon for the type of video input signals the circuit needs to handle to go slightly over 1Vpp, so it may actually be nice to have a bit of head room I guess.
Good to know that at least in theory the circuit stands a chance of working. Now to build it and see what happens in reality... :-)
Thanks again,
Joris