Post Go back to editing

ADA4950 single-ended input with DC-offset to differential output AD9094

Category: Hardware
Product Number: ADA4950

Dear support,

I have some difficulties understanding the implementation of the ADA4950 in a single-ended to differential setup when the single-ended input has a DC-offset. 

I have a single ended input signal (relatively low frequency) which can be anything between 0 and 1.8V. This needs to be converted to a differential signal to be connected to the AD9094. 

I need a gain of 1...this is the circuit which I thought would work (see screenshot) but after some reading online I am a bit doubtful as people mention that a DC-offset on the input could cause issues on the output common mode voltage(?).

The VOCM pins are connected to the common mode output pin of the AD9094 ADC. Would this circuit convert the 0 to 1.8V single-ended input to a 1.8V differential peak-peak output voltage with a common mode voltage which is setup by the ADC? Or am I doing something wrong?

Thank you!

Top Replies

Parents Reply Children
  • Hi Peevee,

    Thank you again for your response! I have updated the schematic according to your insight and now have the following:

    I have AC-coupled the input and routed it to INB+ (because when routing it to INA+ the output signal seemed to be half the input signal and INB+ amplifies it by 2). By having a 5V power supply with a VOCM of half this power supply (2.5V) the swing is well within the range of the amplifier.

    Then I AC-couple the output of the amplifier and provide ADC+ and ADC- to the input of the AD9094. As you suggested I will use the internal common mode biasing of the ADC.

    What do you think of this?

  • Hi Peevee,

    My apologies for asking this much of you but would you be able to take a look at the schematic I posted here yesterday today and have a quick look on how I've now implemented it?

  • Hi MikeHuisma,


    I have AC-coupled the input and routed it to INB+ (because when routing it to INA+ the output signal seemed to be half the input signal and INB+ amplifies it by 2). By having a 5V power supply with a VOCM of half this power supply (2.5V) the swing is well within the range of the amplifier.

    The AC coupling seems okay. About the signal being half, this is due to the resistor combination R5 to R10 before the ADC+/- .

    If you try to probe the OUT+/- pins you should see proper Gain = 1 if you're connected to INA+

    Best regards,
    Peevee