Hi folks,
I'm facing issue with the AD9238 dual 12-bit ADC. The following settings I've used are:
REFT_A and REFT_B short with recommend decoupling circuit
REFB_A and REFB_B short with recommend decoupling circuit
VREF = 1V
SENSE = 3.3V
MUX_SELECT = 3.3V
SHARED_REF = 3.3V
DCS_DUTY_CYCLE = 3.3V
DFS_OUT_FORMAT = GND
OEB_A and PDWN_A = GND
OEB_B and PDWN_B = GND
Thus, the data acquired on channel B (blue) is not as expected, but channel A (green) is correct, as you can see at image below.

The left axis if digital value and x axis is point number.