Hi, My customer needs an ADC interface that works for UHF, C-band, and S-band applications. Please review the attached schematic and suggest if any changes are to be made.
AD9280
Production
The AD9280 is a monolithic, single supply, 8-bit, 32 MSPS
analog-to-digital converter with an on-chip sample-and-hold
amplifier and voltage reference....
Datasheet
AD9280 on Analog.com
AD9208
Recommended for New Designs
The AD9208 is a dual, 14-bit, 3 GSPS analog-to-digital converter (ADC). The device has an on-chip buffer and a sample-and-
hold circuit designed for low...
Datasheet
AD9208 on Analog.com
Hi, My customer needs an ADC interface that works for UHF, C-band, and S-band applications. Please review the attached schematic and suggest if any changes are to be made.
SYNCINB+/- are typically terminated with 100ohm if it is not terminated on the FPGA side. In the schematic, it shows that SYNCINB+/- are connected to SERDOUT. SYNCINB should be connected to FPGA SYNCOUT.
SYSREF is typically DC coupled.
Judy
SYNCINB+/- are typically terminated with 100ohm if it is not terminated on the FPGA side. In the schematic, it shows that SYNCINB+/- are connected to SERDOUT. SYNCINB should be connected to FPGA SYNCOUT.
SYSREF is typically DC coupled.
Judy