Hi, My customer needs an ADC interface that works for UHF, C-band, and S-band applications. Please review the attached schematic and suggest if any changes are to be made.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD9280
Production
The AD9280 is a monolithic, single supply, 8-bit, 32 MSPS
analog-to-digital converter with an on-chip sample-and-hold
amplifier and voltage reference....
Datasheet
AD9280 on Analog.com
AD9208
Recommended for New Designs
The AD9208 is a dual, 14-bit, 3 GSPS analog-to-digital converter (ADC). The device has an on-chip buffer and a sample-and-
hold circuit designed for low...
Datasheet
AD9208 on Analog.com
Hi, My customer needs an ADC interface that works for UHF, C-band, and S-band applications. Please review the attached schematic and suggest if any changes are to be made.
SYNCINB+/- are typically terminated with 100ohm if it is not terminated on the FPGA side. In the schematic, it shows that SYNCINB+/- are connected to SERDOUT. SYNCINB should be connected to FPGA SYNCOUT.
SYSREF is typically DC coupled.
Judy