Post Go back to editing

The reference circuit of ADA4930-1, the driver chip of AD9634 chip

Category: Hardware
Product Number: ADA4930-1


According to the driver circuit design provided in the AD9634 chip manual, the resistance and feedback loops of the ADA4930-1 chip are very different from the resistance and feedback loops in the circuit design provided in the ADA4930-1 chip. The specific difference is shown in the figure below. The RG resistance value in the figure does not match the one described in the ADA4930-1 chip manual, and the circuit designs in the two chip manuals are different. How should this problem be solved?

Parents Reply Children