Post Go back to editing

AD9864 settling time

Thread Summary

The user inquired about the minimum number of frames per symbol for the AD9864, considering a 3LSB settling time. The final answer indicates that the group delay is 7-8 clock cycles (relative to output IQ rate), with a 3-sample delay from the FIR filter and a 4-sample delay from the SSI port. The user clarified that the IQ output will start changing after 4 IQ conversions and stabilize within 11-12 conversions, suggesting a valid symbol every 8th framed IQ conversion pair. The user also asked about potential obsolescence and modern alternatives for the AD9864.
AI Generated Content
Category: Hardware
Product Number: ad9864

It appears possible to pipeline readings through the AD9864 signal chain,  the next symbol can be presented to the input a couple of frames before the present reading starts to change as a result. From tests it appears to take around 11 frame periods to settle to the new value.  I am not au fait with digital filters,  is there a way of determining the minimum number of frames per symbol assuming instantaneous input change and qualifying settling to (say) 3lsb?.  Perhaps this is not documented because it is a standard formula for the filter chain, tabulated somewhere? (if so where?).  

Is there an Analog Devices simulation package one should use to explore this?, it seems odd that it is not (AFAICT) included in the data sheet.

Thanks

Ian

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.