Hi folks,
I am looking for some advice on the design of drive electronics for the AD9434, specifically when considering using the AD8335. The AD8335 is a device I've used before, however this was when driving the ADC3424 from TI which provided schematics for general drive electronics, pictured below:
In the above circuit, the AD8335 was used to provide the source. I would like to continue using the AD8335 as a driver for the AD9434, however I am not sure what the best option for drive electronics would be. From the AD9434 datasheet, the following configuration seems most similar:
It may also be important to note that I am planning to anti-alias using a passive filter directly following the outputs of the AD8335. Any advice regarding this application (and frankly regarding ADC drive electronics in general) would be much appreciated.
Thanks,
Lee