Hi ADI,
We need an ADC setup to sample a single-ended IF signal. We are considering the AD9635 as the ADC with the recommended ADA4927 as driver and to perform the a single-ended to differential conversion.
The IF signal has beat frequencies down to 1 kHz and up to 12 MHz and the plan is to do baseband sampling.
1) Is this a feasible setup?
2) I can't seem to find an example of any of the recommended driver amplifiers (ADA4927 or ADA4938) driving the AD9635. Can you point to an example?
Thanks, Claus